Tool/software:
Hello!
Are there any possible concerns with the circuit below? (e.g. sneak current)
Pull-down resistors of inputs are added to the typical application and connect EN* to Device GND and all others to Module GND.
According to SLVAE55, I thought the current would flow like the blue arrow.
Is it OK if the Absolute Maximum Ratings of Ignd(-50mA) is satisfied when reverse battery?
https://www.ti.com/lit/an/slvae55/slvae55.pdf?ts=1718593022949
Thank you