This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14010A: About circuit design using LMR14010A

Part Number: LMR14010A
Other Parts Discussed in Thread: WEBENCH-CIRCUIT-DESIGNER

Tool/software:

I would like to know about circuit design using the LMR14010A.

When I designed a circuit previously, I looked at the datasheet (SLUSD87 –MARCH 2018).

In the circuit described in the Typical Application at that time, "Cboot" was connected to the "SW" terminal, "D1", and "L1".

The above terminals are also connected in the circuit diagram designed using "WEBENCH-CIRCUIT-DESIGNER" on the web.

However, in the updated datasheet, "Cboot" is only connected to "D1".

When I run "WEBENCH-CIRCUIT-DESIGNER" again, the output circuit has "Cboot" connected to the "SW" terminal, "D1", and "L1".

Please tell me the correct connection.