Tool/software:
Hi Expert,
My customer is evaluating UCC5880-Q1. Some questions need your support.
1. Regarding to the nFLT1 and nFLT2 behavior, Table 7-3 in datasheet shows the fault condition and corresponding recovery operation. But I still not clear for the nFLT1 behavior if the fault is removed. After the fault(like VCC2 UVLO fault) is removed, does the nFLT behavior will be latched until fault bit is cleared? Or the nFLT will be recovered to high level once the fault is removed?
2. For the VCC2 OVLO fault, customer feedbacked that they cannot get the same phenomenon mentioned in datasheet. You can find their test description as below. May you kindly check the reason?
Set CFG2[OVLO2_TH]=00b, ACT1[OVLO2_ACT]=11b, -> modified the R73 resistor to 81K(18.9V on VCC2) -> read FAULT2[OVLO2_FAULT]=0b and OUTL not be pulled low.
They also tried to increase the VCC2 voltage to 22V, but the behavior still not as expected. They can get VCC2 OV fault in fault register several times with tried many times.
Register value:
UCC5880 device marking:
Thanks!
Ethan Wen