Tool/software:
Hello,
In our application, we need a MCU and DC-DC to make a adjust power supply unit with 36V input and 5-30V 10A dynamic output, and from https://www.ti.com/lit/an/slva861/slva861.pdf, we think we can use LM61495 for our design, however, we want to confirm about following questions.
- In the https://www.ti.com/lit/an/slva861/slva861.pdf, it suggest using a vdac connect with FB of DCDC, and about the caculate of Rset, for LM61495, the value of Rset should be what? and the vDAC need how many output ability? can stm32g431 dac working enough for it?
- For the dynamic adjusting, when the DAC output to FB, the output will change, and for example, when we want to change output voltage from 5V to 15V, we have to decrease the DAC voltage to let Vout increase. should I use a div to caculte the DAC (15V/1V, and change the DAC output 1/15*Vout, so that when Vout increase to 15V the Vfb is 1V) or just a value less than 1V and use something like PID to change it(change the DAC to 0.9V and when the Vout is near 15V ,change DAC back to 1V)? because accroding to the datasheet, the Vfb have a limit range, if we use the method 1 it seems will occur a fault of LM61495.
- Is there other DC-DC chips can use for our application? with 36V in and 5-30V out 10A. and can support dynamic adjust when working?
Thanks,
Siyu