Other Parts Discussed in Thread: LM51551-Q1, LM51551, LM5155
Tool/software:
Dear Sirs,
we are not sure if we can use LM51231-Q1 to design a rather unusual boost converter:
Vmin = 2.5V
Vnom = 3.3V
Vmax = 3.7V
Vout = 20V
Iout = 3A
It will be used for driving a 20V BLDC motor, so output ripple is not much of concern. Also the output will only be used for short periods of time (max. 2s). But we are very space constrained.
Any concerns from TI for such a setup?
Many thanks
Joern Ihlenburg