Tool/software:
Hey all,
I've got a peculiar situation here. The output of this buck is set to 6V through the feedback resistors, but I need to have 8.2V on the output temporarily for One Time Programable programming during production.
So my question is if I have 11V or greater on Vin, 8.2V on the SW pin, and the regulator is set to output 6V, do you expect for there to be any potential issues with this for the device? I'm assuming the LM5168-Q1 will just be at a 0% duty cycle until the output voltage goes under the set output voltage of 6V. This will be for a short duration.
Thanks,
Robert