This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62903: Issue with Low-Vin-Buck Simulation in PSPICE for Power Supply Design

Part Number: TPS62903

Tool/software:

Hi Power Management, I am a FAE intern working on a power supply design project and have been running into some issues with my simulations. Could you assist me in knowing where I could be going wrong with my design or if there could be a simulation issue? I have pasted the schematic below as well as the reasoning for the component selection and configuration.

-12V nominal supply as desired nominal input and in range (3V-17V)

-10 micro-farad cap as specified in applications schematic in data sheet

-Mode/S-conf resistor of 11.0K because the desired switching frequency is 1MHz, in auto PFM mode, and uses external feedback for voltage regulation

-SS/TR capacitor of 30pF to get lower soft-start ramp time

-PG hooked to ground (wouldn't let it float in PSPICE simulations)

-SW inductor of 2.2 micro-henry and decoupling capacitor of 22 micro-farad as specified in applications schematic in data sheet for recommended LC filtering for 1MHz switching frequency

-R1 of 113K and R2 of 24.9K to get 3.322V output (~3.3V)

Also, would a 20% tolerance on the inductor and 10% tolerance on the capacitors be appropriate for EVM testing?