Other Parts Discussed in Thread: UCC28950
Tool/software:
Hi
Do you have any recommended power solutions for the specifications below?
I want to implement them in analog, not digital.
-SPEC-
Input: DC 300V
Output: 65V 83A
non isolation
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi David,
Thank you for reaching out.
This is definitely out of scope for UCC28730 and other flyback controllers.
I think you should check out phase shifted full bridge for this application. UCC28950/51.
Please open a new post under this IC name so that experts for this controller can take a look into this.
Regards,,
Harish