This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FLYBUCK-FLYBACK-DESIGN-CALC: Query on power stages design for AUX power

Part Number: FLYBUCK-FLYBACK-DESIGN-CALC
Other Parts Discussed in Thread: UCC28061

Tool/software:

Hi,

We need to design Audio system with 4 amplifiers each of 150W so total load of 600W.

I need to design FLYBACK converter for stepping down 380Vdc generated from UCC28061 PFC controller into the AUX supplies of 15V (also required for Bias supply of IC), 12V (internal) and 48V (POE)
i prefer to have PSR, CCM/QR conduction with variable frequency switching.

Let me know if there are any better solutions available for the requirements.

Thanks,

Amit