Other Parts Discussed in Thread: , TPS546D24A
Tool/software:
Dear Sirs and Madams,
We are currently mounting the TPSM8D6C24 on a board and checking its operation.
When the output voltage was set to 800mVdc, the output ripple voltage was observed with an oscilloscope and found to be a sine wave of approximately 70mVpp with a period of approximately 50kHz.
Because the switching frequency is set to 650 kHz, it is believed that with 2-phase operation the ripple voltage period will be 1.3 MHz, and that the low-frequency operation of approximately 50kHz is unrelated to switching.
So, I would like to confirm for the operation of the switch node of the TPSM8D6C24, but the SW_A/B terminals assigned to the bottom of the TPSM8D6C24 do not have a through-hole on the board, so they cannot be measured with a probe.
Is there a way to confim the switch node from the surface mounted on the TPSM8D6C24 module?
Regards,
MM