Other Parts Discussed in Thread: TPS22998
Tool/software:
Hi Team,
TPS26601 as load switch.
Vin/Vout=48V
Iout/Ilimit=0.7A
I_fastrip= 1A
What is the Cout capacitance to be used in design?
Regards,
Vidhya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Vidhya,
In power designs, Standard recommendation for Cout is 1uF per 1W of load.
You can use in the range from 33uF to 47uF
Best regards
Rakesh
TPS22998 handled by different engineer. can you please post new thread on TPS22998
Cin can be as small as 0.1uF for TPS26601
Cout can be from 0.1uF to mF range based on the transient support needs of the load. There is no Cin:Cout ratio dependency for TPS26601