LM5148-Q1: Solar - PV optimizer Design & Development -Power Topology Selection

Part Number: LM5148-Q1
Other Parts Discussed in Thread: LM5175, LM5176

Tool/software:

Hi there,

Currently I am working on development of MPPT based PV optimizer for solar power optimisation,

The Power level of Power optimizer is 700Wp [Voc= 52V, ISC = 15.5A.( Vmpp = 50V, Impp=14A)] Which power topology is more suitable in non-isolated topology area?

With lot of literature study, I have come across buck, buck-boost, cuk.  

Which is the best suitable power topology, that I should prefer as far as the solar domain concerns.

In in case of buck-boost (which one to select buck-boost or cuk)?

Thanks in Advance!!!