Other Parts Discussed in Thread: TPS3760-Q1
Tool/software:
Hello Expert,
Could you please tell me how to use following hysteresis information?
Datasheet said as below.
However, this calculation seems that there are some miss match against other reset ICs and specification.
For example, to estimate min value, it probably used 5% as 7mV - 7mV*5% = 6.65mV.
If I used 0.5%, at least it should be 7mV -7mV*0.5% = 6.965mV.
Moreover, the other reset ICs hysteresis "accuracy" information is defined as below.
Then, hysteresis min/Max is calculated as Hysteresis voltage(Vth[mV]*hys[%]) * Accuracy(e.g.7mV*(+-1.5%) = 6.895mV/7.105mV).
But TPS3842-Q1's hysteresis calculation is completely different against the other device.
So I'd like to make sure about how to calculate hysteresis min/Max.
Best regards,
Kazuki Kuramochi