Other Parts Discussed in Thread: USB2ANY, TPS55289, TPS55288
Tool/software:
The GUI can connect with the USB2ANY , but can't connect with the EVM through I2C whatever the addr is 74H or 75H , the TPS55288EVM-530 has the same problem .
the USB2ANY's fireware version is 2.8.2.0 .
the USB2ANY Explorer doesn't show errors , I can light the 3.3V or the 5V .
When I connect the EVM , I move the jumper of JP1 to the ON position.
the GUI is as below: