This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6594-Q1: AMUX_OUT pin goes high when PMIC put to MCU only mode

Part Number: TPS6594-Q1

Tool/software:

Hello,

I am trying to put PMIC to MCU only mode on our custom board. Power rail connections are as per the recommendations.

Before changing to MCU only mode, I set AMUX_OUT to low, this works. But when changed to MCU only mode, AMUX_OUT automatically goes to high. What is the reason?

Looks like MCU is not running after switching to MCU only mode. Does PMIC detected any errors/interrupts and move to safe state?

MCU related rails show at correct voltage levels, and SoC rails are zero volt. But looks like MCU is not running after changing to MCU only mode.

As JTAG connection is lost, do not know how to check what's happing in MCU. Trying to use AMUX_OUT state changes to see that MCU is working in MCU only mode. But AMUX_OUT automatically goes to high after MCU only switching and MCU is not running because, MCU cannot change the AMUX_OUT state

  • Hello Raghavendra,

    What TPS6594 part number do you have, this makes it much more clear as the PMIC states.

    How are you setting AMUX_OUT low and from what state is this transitioning from?

    Before changing to MCU only mode, I set AMUX_OUT to low, this works. But when changed to MCU only mode, AMUX_OUT automatically goes to high. What is the reason?

    Depending on the programming for the device, a possibility is that the device is hard coded to enable this resource when transitioning to MCU_ONLY mode as for many safety parts this is needed for coverage.

    Looks like MCU is not running after switching to MCU only mode. Does PMIC detected any errors/interrupts and move to safe state?

    Depends on the SoC & TPS6594 NVM, please provided both part numbers. Yes, when fatal errors are introduced the PMIC will power down in manner reflecting the urgency, transition to safe state, and then attempt another power up. This is dependent on the part number.

    As JTAG connection is lost, do not know how to check what's happing in MCU. Trying to use AMUX_OUT state changes to see that MCU is working in MCU only mode. But AMUX_OUT automatically goes to high after MCU only switching and MCU is not running because, MCU cannot change the AMUX_OUT state

    There are better signals to observe if the MCU is supposed to be active such as the nRSTOUT pin.

    BR,

    Nicholas

  • Thank you for the reply,


    We are using 2 PMIC setup

    TPS65941210-Q1  as PMIC-A and TPS65941111-Q1 as PMIC-B


    AMUX_OUT from the PMIC-A is kept open and measured to check whether MCU still running when enters to MCU only mode as JTAG is lost.

    nINT and END_DRV are low

    nRSTOUT pin is high and nRSTOUT_SOC is low when MCU only mode is entered. 

    MCU rails are active, showing correct voltages and SoC rails show zero volt in MCU only mode.

    My main problem is, MCU is not running when MCU only mode is active though MCU rails seems to ON and nRSTOUT is high. 

    As there are no GPIO on our board connected to MCU domain available outside, I tried to toggle AMUX_OUT to check whether MCU is active.

    I am also measuring I2C data line and do not see any data being transferred from MCU once we enter MCU only mode. To debug periodically reading PMIC register to see activity on I2C. But no activity after MCU only mode.

  • Hello,

    I read NVM registers for both PMICs,

    PMIC-A

    TPS65941210-Q1 => 0x48

    DEV_REV => 0x82

    NVM_CODE_1 => 0x10

    NVM_CODE_2 => 0x04

     

    PMIC-B

    TPS65941111-Q1 => 0x4C

    DEV_REV => 0x82

    NVM_CODE_1 => 0x11

    NVM_CODE_2 => 0x03

  • For the AMUX out, before MCU only mode, i set state to disabled. I can see 0V
    After MCU only mode, AMUX automatically changes to close to 1.3 V

  • Hi,
    Is there any way to still connect JTAG (Trace32) in MCU only mode? 

  • Hello Raghavendra,

    Hello,

    I read NVM registers for both PMICs,

    PMIC-A

    TPS65941210-Q1 => 0x48

    DEV_REV => 0x82

    NVM_CODE_1 => 0x10

    NVM_CODE_2 => 0x04

     

    PMIC-B

    TPS65941111-Q1 => 0x4C

    DEV_REV => 0x82

    NVM_CODE_1 => 0x11

    Thank you, so it looks more than likely this is a TPS65941310 & TPS65941111 setup as we don't offer up a TPS65941210.

    Here's a User's guide on the setup, I'll be referring to this setup: TPS65941310-Q1 and TPS65941111-Q1 PMIC User's Guide for Jacinto™ 7 J721E, PDN-0A

    For the AMUX out, before MCU only mode, i set state to disabled. I can see 0V
    After MCU only mode, AMUX automatically changes to close to 1.3 V

    A transition to MCU only mode will always enable the AMUX to output the reference voltage on the pin. This is programmed into the unit and can not be altered.

    The nRSTOUT pin is the most sure fire way to tell if the power sequence has completed and all of the power rails specified to on for the MCU have been completed as it is the last resource to be asserted high.

    Hi,
    Is there any way to still connect JTAG (Trace32) in MCU only mode? 
    I am trying to put PMIC to MCU only mode on our custom board

    Since this is a custom board, I'm not sure of "Trace32" or the custom board's implementation of JTAG.

    More over how was the MCU only mode enabled, what trigger was done to switch over to MCU only mode?

    Best Regards,

    Nicholas

  • Thank you for reply,
    MCU only mode is triggered via controlling NSLEEP1 and NSLEEP2
    Via I2C, address 0x86 and value 0x02 for PMIC - A (0x48)
    I can see the I2C data line. When interpreted the i2C data on bus, its matching.

  • Hello Raghavendra,

    Thank you, that confirms you are entering the MCU_ONLY mode the intended way.

    I can not confirm if the MCU is on or not due to the custom board configuration as JTAG configuration is dependent on the MCU implementation.

    As far as the PMIC is concerned, the device has all of the MCU rails on and the nRSTOUT pin is high so there's no issue from the PMIC.

    It's best to ask this question in the processor forum.

    Best Regards,

    Nicholas