Tool/software:
What is the range of the input and output voltage?
input voltage: 20V ; output voltage: 50V ; power: 50W ,could it be possible?
Hello,
As long as the appropriate VCC voltage is applied to the UCC28070A controller, it can boost virtually any input voltage to virtually any output voltage, as long as Vout > max Vin.
The voltages are scaled to the input ranges of the controller.
Yes, it is possible to construct a 50W PFC circuit using UCC28070A with Vout = 50V and Vin = 20V. I assume that this is 20Vrms AC input.
Regards,
Ulrich