This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ10501: Faulty regulators overheat, problem fixed by replacing the component.

Part Number: LMZ10501

Tool/software:

Hello,

We are using two LMZ10501 on one PCB. Both are supplied by a 5V Boost.
One LMZ is providing 1V8 and the other 3V3.

We are facing a big issue on this board related to these components. We have around 30% of board failing due to these regulators.
The failure appears on both regulators. The failure can always be fixed by manually replacing the regulator.
When we got a faulty regulator, it usually regulates output as expected but overheat and quickly go off with thermal protection. When the regulator is replaced, the temperature of the regulator does not exceed 40°C at ambient room temperature.

We are not strictly respecting the layout guidelines but yet it does not explain why the issue disappears when we replace the regulators by new one.

I measured impedances between pins to see if there was any short but I did not see any. There are some differences but I don't know if we can learn something from them:

  Impedances between pins for a faulty LMZ10501 1V8 (kΩ)
  Vin Ground Vcon Vout EN Vref
Vin   200 80 460 490 250
Ground     70 46 470 136
Vcon       160 600 123
Vout         500 200
EN           630
Vref            
  Impedances between pins for a working LMZ10501 1V8 (kΩ)
  Vin Ground Vcon Vout EN Vref
Vin   600 490 500 760 424
Ground     70 60 790 141
Vcon       205 777 125
Vout         830 280
EN           810
Vref            

We also send some PCB the X-Rays to ensure that the soldering beneath is fine. On both regulators they were fine whereas all PCB sent had issues with at least one of the two regulators.
On the X-Ray though, we discovered that we had two different versions of the regulators. We can see that the IC inside is very different:

I can share with you schematics, board layout and further measurements I made in private.

Best regards