This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Experts
I am using the TPS5450DDAR step-down converter to obtain 3.3V from 12V. It powers a set of LEDs and the microcontroller on the PCB. Please see the schematic below. The issue is that radiated emission peaks are above the limit. Any suggestions for PCB modifications to improve this would be highly appreciated.
EMI Using near field probe
FCC 15B RE test output
Looking forward to seeing your response
Best regards
Dushan
Hi Dushan,
You could try replacing C70 with a 100nF capacitor. Also You could try different shielded inductors from other vendors (Coilcraft, TDK, Murata, etc) and see if that helps.
Thanks,
Andrew
Thanks for your prompt response. I will try and send you the results
Best regards
Dushan