Other Parts Discussed in Thread: CC1310
Tool/software:
hi.
I am currently developing with “CC1310 LAUNCHXL KIT” and I have a question while I am developing. In CC1310 I enter Sleep Mode and I used to plug in the debug wire and measure the current and 2.5mA was measured, but when I remove the debug wire and measure the current, 0.4mA was measured. But when I look at the TI CC1310 DATA SHEET, it says that 0.7 uA should be measured when in sleep mode. My question is that currently I am using “Power_releaseConstraint(PowerCC26XX_SB_DISALLOW)” as the code to enter sleep mode;
Power_setConstraint(PowerCC26XX_RETAIN_VIMS_CACHE_IN_STANDBY);
PowerCC26XX_standbyPolicy();” I wrote this code, but is there a better way? And “Power_sleep(PowerCC26XX_STANDBY);” and “Power_releaseConstraint(PowerCC26XX_SB_DISALLOW);” I want to know the difference between these two codes, and is it okay to use Power_setConstraint(PowerCC26XX_IDLE_PD_DISALLOW); when I declare to use standby mode like the code above?
Besides the above method, can you tell me if there is any code instruction to decrease the current value of CC1310 close to SLEEP MODE?