This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
What is minumum load current of LM51571-Q1.
Webench Power Designer Tool is designed 100mA circuit.
There is no fault.
İf load current is only 5mA. Do this circuit work properly.
Best Regards.
Hi zabbza,
Thanks for reaching out.
LM5157 does not have a minimum load current.
At some point at low load, the device will start to skip cycles to avoid the ouptput voltage from running away.
Best regards
Moritz