Other Parts Discussed in Thread: PMP15038
Tool/software:
Hi,
the goal is to use the LM5171 to control the charging/discharging current and cutoff-voltage of a connected LV-battery via a DAC.
For example: target LV-Voltage is set to 13.8V, but at the same time the output current limit should be dynamically adjusted from for example 100mA to 30A via a DAC.
(digital potentiometers should not be used in this project)
Output voltage at LV: this seems to be quite easy, by controlling the VSET of the outer loop via the DAC
Output current at LV: this looks more complicated to me, because we still would like to use the outer loop error amplifier to prevent overvoltages/overcharging,
but compared to the reference designs, we would like to dynamically adjust the limit of the output current.
The eval-board is using a fixed resistor divider which from my understanding is just providing a fixed current limit
and the alternative circuit of the eval-board (by jumper-setting) is ignoring the outer voltage loop and let the user handle all kind of voltage controls.
Is there an easy way to implement this adjustable current limit via a DAC, while keeping the outer voltage control loop?
Thanks