This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Customer is looking for a LDO to meet below condition and >28V rating for FuSa SIL3 motor drive power
Condition: 5.5Vin to 5.0Vout/2A or 3A ; Since it's for safety power, the input voltage derating has to be > 28Vin.
Could you help to suggest a suited one! Very thanks.
Regards
Brian
Hi Brian,
I think LM1084 would be a good fit here since it is both adjustable and has a fixed 5Vout version and can handle up to 29Vin and 5.5A Iout.
Adjustable version: LM1084ISX-ADJ/NOPB
5Vout version: LM1084ISX-5.0/NOPB
| LM1084 | |
| Iout(Max)(A) | 5.5 |
| Vin(Max)(V) | 29 |
| Vin(Min)(V) | 2.6 |
| Vout(Max)(V) | 27.5 |
| Vout(Min)(V) | 1.25 |
| Fixed output options(V) | 3.3, 5 |
| PSRR @ 100 KHz(dB) |
30 |
| Noise(uVrms) | 38 |
| Accuracy(%) | 1.5 |
| Dropout voltage (Vdo)(Typ)(mV) |
1300 |
| Iq(Typ) (mA) |
5 |
| Output capacitor type | Non-Ceramic |
| Thermal resistance θJA(°C/W) |
23 |
| Operating temperature range(C) |
-40 to 125 |
| Package size: mm2 | 155 mm2: 15.24 x 10.16 (DDPAK/TO-263|3), 47 mm2: 4.58 x 10.16 (TO-220|3) |
| Rating | Catalog |
Regards,
Andres