Other Parts Discussed in Thread: LM5012, LM5160-Q1
Tool/software:
Dear TI experts,
My customer considers LM5012-Q1 for their new project.
They use PoE for the input of LM5012-Q1. So the input voltage would be 24V or 48V.
And the output voltage is fixed to 24V.
I think that 48V input voltage would be fine, but if the input voltage is 24V, input and output voltage are the same.
How can I expect the voltage drop if the input voltage and output voltage are same as 24V? Can I find any specification on the datasheet?
- If the voltage drop is too large, Could you recommend other IC which is similar to LM5012 and have no voltage drop with such a situation?
Input voltage is 24V and 48V, output voltage is 24V fixed. and maximum output current is 0.65A. They prefer Automotive qualified parts.
Best regards,
Chase