Other Parts Discussed in Thread: BQSTUDIO, , EV2400, , GPCCHEM,
Tool/software:
Dear Ti Engineer,
I am new to BMS chip.
I am also new to battery and BMS.
I use bq34z100, EV2400 and bqStudio.
I don't know many parameters used in bqStudio.
So I don't know which parameter to use and how much value to input, so I would like to get help.
A. The system specifications we use are as follows: =================================================
1. Test environment:
Actual load to be used: 330W(max)
Test load: 6 ohm /50W
Circuit: bq34z100EVM board, R30(Current sensing resistor) = 0.01 ohm / 15W
2. BATTERY specifications:
Maker: Shenzhen Cyclen Technology Co., Ltd / China
Model: CY-LFP-1260t
Spec.: 12V/60Ah
Chem. : LiFePO4
(Detailed specifications are attached in the file)
3. Charger specifications
Maker : MEAN WELL /
Model : NBP-450-12
Spec : 420W, Max Ouput:25A
(Detailed specifications are attached in the file)
B. Inquiry:
==============
1. Please tell me how to select the type and value to set the parameters of the BMS chip in bqStudio.
2. I don't know the Chemical ID / It is not in the list
For now, I set the Chemical ID to 0421 in the test.
Can I use a similar temporary ID for the test?
3. When charging, the SOC value is displayed
(of course, it is not the correct value because the parameter setting is not correct),
but when discharging, it is displayed as 0. Why is that? Please give me a solution.
I'm looking forward to a good answer.
Thank you.
Best Regards,
Hwang, Seognjin
email : sjhwang@volkkorea.com