Tool/software:
Hi, E2E-
I'm developing a replacement for an old 20S Ni-Cd pack found in a piece of test equipment, and I am considering using a 6S Li-Ion stack with a pair of BQ77915s. The "catch" is that this pack needs to be ground referenced at the center of the stack such that split positive/negative voltage rails are available on the output. Similarly, it will charge using a set of +13 / 0 / -13 V supplies. Any issues using the BQ77915 in such an application? Please let me know if this question isn't clear, and I can attach a rough schematic of what I have in mind.
Thanks,
-Erik