This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Nikhil,
Please be sure that the effective capacitance on Cout is at least 15uF. If you do not have a BIAS supply to connect to the BIAS pin then you do not need to place a capacitor on the BIAS pin to GND. The schematic looks good otherwise.
Thanks,
Stephen
Hi Stephen ,
Thanks for the feedback.
if i am using Vin=1.2 V and Vout= 1V @2.5A , please confirm if the same design is okay to proceed. (without bias V and CP enabled)
thanks,
nikhil
Hi Nikhil,
Yes, Vin = 1.2V and Vout = 1V while using the charge pump will be fine.
Thanks,
Stephen