Tool/software:
Hi,
I'm planning to use TPS61040 for my below requirement:
These are the inputs I've given to Webench.
VIn(Min)= 4.8V
VIN(Max) = 5.5V
Vout=7V
Iout(Max) =50 mA but typical would be very small around 10mA.
When I tried to take design from TI Webench, it is giving me very high value of inductor which 22uH. Is it possible to use low inductor values such as 6-10uH.
Also what is the minimum switching frequency of TPS61040.
Thanks,
Yogesh