Part Number: UCC28730-Q1
Tool/software:
I have designed a 23 W Flyback-Converter with 1Outputs with a Inputvoltage of 250-800V and an Outputvoltage of 11V/2.1A.
I am now trying to put the PCB in operation, but I am facing unstable switching behaviours. The controller keeps restarting。I think the shutdown was caused by a reported fault。
There is only one restart pulse(4.14us) as the green line(CH1:Vds CH2:Vdd CH3:Vout)。

maybe the OVP or oc or uvlo fault.The actual test current did not reach the overcurrent point, and a 120pf capacitor was also added to the CS pin, which seems to have little effect(CH1:Vgs CH2:Vaux CH3:Vout CH4:Ids)。
the voltage of Vaux exceed 22.5V ,after the tlk-reset time, The voltage of Vaux does not exceed the overvoltage point(21.5V RS1=121k RS2=33k),so
I don't think it's an overvoltage fault。I noted that the Vaux ringing Below Ground Can Trip UVLO,

The actual voltage oscillation will also be lower than 0,Do you think UVLO triggered the system shutdown and how to solve it?What fault can cause a restart with only one pulse?