Other Parts Discussed in Thread: BQ25792, , , BQ25756, PMP41062
Tool/software:
Hi,
I am currently working on board design with TPS25751SRSMR on our custom board for PD application with battery charger BQ25792. This PD controller is suppose to be pre-configured for this battery charger and I was told before that no such firmware is required if we are going to use these two together. Please help me to clarify these 2 points:
1. Can you please confirm that if ADCIN pins that are suppose to be configured on each power ON or this is only required for the very fist time? I am asking this as we would like to not add any EEPROM on-board and would like to use USB DP/DN connected between PD controller and USB-C to be configured via TI customization tool.
2. Please note that we are not adding any external embedded controller but as per this configuration table "Always Enable Sink" is supported when we have external embedded controller, the "Negotiate High Voltage" is not valid to use with any supported battery chargers and "Safe Mode" is only if we have EEPROM. To me it looks like Negotiate High Voltage is the one to go with but I am confused when it states that "This configuration is not valid to use with any supported battery chargers". Please clarify and help me to use the correct configuration based on our application.

Please note that this is our intended use with only PD controller and battery charger without and EEPROM or External controller:

Kind regards,
Mat