Tool/software:
Hello,
The chip also has a thermal turn-off of the thermal swing function, the swing T(hys) is 10℃, but for our actual equipment, the load on the PCB board will be opened and closed at any time, which will lead to the entire onboard temperature is changing, it is easy to turn off the output because of the thermal swing function, whether the thermal swing function can turn off the detection? However, it is also written in the following figure that Thermal Behavior After Short to GND, so does the diagnosis start when the output is short-circuited to the ground, The temperature change has no impact on normal use?