Tool/software:
Hi,
I am designing a 5kW phase-shifted full bridge regulator using the UCC28951. I am having trouble maintaining soft switching on my A/B transistors, which is preventing me from reaching high loads. I can achieve ZVS at light loads, but lose it as my currents increase which seems backwards to me.
On my primary side, I am using silicon carbide FETs (~20pF Coss) with parallel silicon carbide diodes (~20pF junction) to mitigate reverse recovery. Clamp diodes are also silicon carbide.
I've noticed significant asymmetry in my AB and CD legs on transitions - more significant than in any reference material I can find. This is coupled with shim inductor current that also looks inconsistent with reference material. AB transitions cause a complete depletion of shim inductor energy that does not seem to line up with the capacitances I have.
I attached a simplified schematic and a screenshot of the behavior at 20% load showing my AB and CD transitions as well as shim inductor current.
My question is: does my AB waveform look normal and I just need to do some tuning, or is there likely something else wrong in my system?
Thanks!
Brian