Tool/software:
Hello,
is the datasheet named maximum load current for all channel or for one channel.
Means Load Current of 2.5A resulting in 4 times 2.5A in total 10A for all channels or in 2,5A / 4 channel = 0,625 A per channel?
Thanks
BR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
is the datasheet named maximum load current for all channel or for one channel.
Means Load Current of 2.5A resulting in 4 times 2.5A in total 10A for all channels or in 2,5A / 4 channel = 0,625 A per channel?
Thanks
BR
Hi BR,
The maximum load current is for each/one channel. So, each channel ideally can handle 2.5A but because of mutual heating (if one FET is on, the other experiences a slight temperature change) if all four channels are being used, it will probably be around 2A.
Thanks,
Rishika Patel