This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dearn TI Team,
1) The table 6.2 shows output HO and LO pins are High, if both the inputs are High.
2) section 5.1, the HS DC minimum voltage is mentioned -1V, is it correct or -10V.
please give the clarification, Is it correct or printing mistake.
Hi Anil,
1. Yes, both outputs are high when both inputs are high. This device does not have cross-conduction protection (interlock), but if you would like a device with interlock, then we recommend the UCC27301A.
2. Yes, -1V is the absolute minimum the HS pin can handle at DC.
Thanks,
Rubas