This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi sir,
I want to design power supply using LM5180-Q1 IC which will have 2 outputs say 5 Volt 500 mA each. Can you suggest suitable fly-back transformer for this. Please look into this
Thanks & Regards
Aditya Mene
Hi Sir
First of all thank you for your valuable response. We are planning to design this supply for operating temp from - 40 °C to + 85 °C. Here I have attached the input output specifications for the same will you please suggest some fly-back transformers for the same.
Thanks & Regards
Aditya Mene
1106.LM(2)518x PSR flyback converter quickstart tool revB.xlsx
Hello Aditya
I am sorry. Your application is not supported by LM5180/81/LM25180/3/4 due to the power limit at min VIN and Abs max VIN.
Please consider using LM5185. Please download the Quick Start at https://www.ti.com/tool/download/LM5185-DESIGN-CALC , input your electrical specifications and component selections. Please use ZB1051 as a starting point and refer the datasheet at https://www.coilcraft.com/getmedia/6a364174-fe48-4806-af5b-ff882c0f5ee8/zb105x.pdf. If required, please refer other transformer options here at https://www.coilcraft.com/en-us/products/transformers/power-transformers/no-opto/
Please create a new post if you have further question about LM5185.
Customers are responsible for component selections and layout design, as well as validating and testing their design implementation to confirm system functionality.
-EL
First of all thank you for your valuable response. As you have suggested Coilcraft ZB1051 transformer for LM5185 IC can you suggest any transformer from Wruth for same application.
Thanks & Regards
Aditya Mene