Tool/software:
Hi,
As the title says, I'm using a bq4050 for a 4S BMS application. The circuit is basically a copy of the application example shown on the datasheet. During testing, we need to manually turn ON/OFF the charge and discharge FETs. We realized that, when in manual mode (FETEN=0), the discharge FET is off and VBAT > 16V, the charge FET cannot be manually turned ON. When sending the command 0x001F, the bq4050 acknowledges the command and changes the internal flags to show that the charge FET is ON (CHGEN = 1) but in reality, the charge FET remains physically off.
Is this a bug in the bq4050 IC? Will this effect the safety feature of the BMS (ex, re-enabling charging after it was disable for safety).
Note:
1. While in the condition where the flags are showing the charge FET is on (CHGEN=1) but in reality it is physically off, if we enable the discharge FET (mac command = 0x0020), the charge FET does than physically turn ON.
2. Turning OFF the CHG FET always works in any condition.