This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dear TI support,
We are using TPS610333QDRLRQ1 as BOOST from 3V3 to 5V with current output load up to 0.21A
Here below the detailed schematic
We observe 2 behavior which are not expected according to the configuration mode chosen
1-Output voltage ripple of around 170mW and our target is below 100mV
2- Big overshoot and undershoot in the switching frequency captured at inductor testpoint
Could you please check the schematic and setting value and provide us with the good configuration and corrective values for the following objectives :
- Reduce the output voltage ripple below 100mV
- Eliminate Undershoot and overshoot in the switching frequency (inductor)?
Thank you for you quick feedback
Best regards,
Karim
Hi Karim,
The schematic looks ok, I suspect that the large ripple and large ov/uv is introduced by improper measure method.
To achieve the most-accurate, noise-free measurement, a low-inductance probe should be used between the SW node pin / VOUT node pin and the power GND pin on the IC.
Please refer to these two ANs as more details about the correct measure method and double check.
Understanding the Absolute Maximum Ratings of the SW Node
Measuring and Understanding the Output Voltage Ripple of a Boost Converter
You can also take the waveforms in d/s as a reference.
Regards,
Nathan