This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS552872-Q1: Schematic Review

Part Number: TPS552872-Q1

Tool/software:

Hi Team, 

Could please review the design and share your comments? 

Design Requirements

Input Voltage : 9-16V

Nominal I/P Voltage : 12V 

Output Voltage : 12V 

Output Current : 2A 

Output Power (Max) : 24W 

Ambient Temperature (max) = 85°C 

Application : Automotive 

/cfs-file/__key/communityserver-discussions-components-files/196/TPS552872_2D00_Q1-Schematic.pdf