Other Parts Discussed in Thread: TPS25751
Tool/software:
Greetings -
I recently received the TPS26750EVM and have had minimal, boarding no, luck programming the micro on the EVM.
I have tried different USB-C cables, different browsers, baud rates, offline desktop app and different desktop systems no less than one hundred times, with one successful attempt.
Given that it has worked once and the progress bar when attempting moves from 10% to 40%, to 70% then fails, its clearly communicating with the micro but for whatever reason it fails after 70%.
I only have one EVM as TI limits what one customer can purchase at at time and puts a 30 day waiting period between requests, so I'm unable to test another assembly.
Any help/guidance would be greatly appreciated.
Best,
-Chris