Tool/software:
Hello everyone,
I’m trying to simulate the LM5149 in PSpice for TI 2024. I’ve downloaded the LM5149-Q1 PSPICE Transient Model from the TI website and followed the provided steps.
After loading the file, I opened the schematic and ran the simulation without making any changes. The simulation completes, but the output voltage is consistently 6V, even though the circuit is designed for a 5V output with a 12V input.
Interestingly, tweaking the feedback resistor values doesn’t seem to affect the output voltage—it remains at 6V. Furthermore, if I increase the input voltage (VIN), the output voltage (VOUT) always appears to be half of VIN.
As someone relatively new to PSpice and electrical simulation, I’m unsure if I’m missing something critical. Has anyone else encountered this issue or can suggest what I might be doing wrong?
Thanks in advance for your help!