This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23730: Regarding TPS23730RMTR dual port POE design question

Part Number: TPS23730


Tool/software:

Hi Sir,

Regarding  TPS23730RMTR dual port POE design, we have below question.

Attached is TPS23730RMTR dual port POE design illustration.

Form attahced file , there are two POE out port. One output is Port1_12V, the other is Port2_12V. Then, it is combined to final 12V output.

Since componets variation for port1 and port2, thus ,it will cause  Port1_12V has 12V +/-5% voltage tolerance and so as to Port2_12V.

In case Port1_12V is at +5% and Port2_12V is at -5% voltage situation, is it possible to let one of the port cause this port over its maximum output power capability  is happened? 

Is this issue occured?

Please advise

dual POE.pptx