Is there any way in which I can run two LMZ14203H power modules in parallel to increas current capability?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ken,
Unfortunately the LMZ14203H modules are not designed to work in parallel. The LMZ23608/10 power modules are specifically designed to do this, but the output voltage maximum is 6V. A load sharing controller such as the UCC39002 may also work.
Regards,
Allan