Part Number: LM2679
Other Parts Discussed in Thread: LM2678
Hi Team,
Posting on behalf of our customer.
I will share this E2E post to our customer so he can reply when needed.
I have an old design (has worked well for many years) based on the LM2676-ADJ that I'm attempting to migrate to the LM2679-ADJ in order to provide a bit more output power.
My problem is that my LM2679 seems to initiate current limiting much sooner than I'd expect. To get started, I set the current limit resistor to 5.3 KOhm, to match the fixed 7A switch current limit of the LM2678, using the 37125/7 equation from the datasheet. (The LM2679's datasheet doesn't really specify a max value for the switch current, at least I can't seem to find it, but I assumed it would be the same as the LM2678.)
Even under lighter loads, say 2-3 Amps, the LM2679 initiates current limit (as evidenced by the output voltage drop and by viewing the switch output waveform). I wouldn't expect that output to require anywhere near 7A from the switch. (Vout is 12V, Vin is 16V for this test). In addition, the current limit function seems so sensitive, that if I so much as put a scope probe on the current adjust pin, it immediately sends the device into current limit. To further test my assumptions on the currents, I replaced the LM2679 with an LM2678 on the same board, and it works great, well past a 4A load.
I can "make it work" by arbitrarily lowering the current limit resistor (need to drop it down closer to 4KOhm), but I really don't want to go there, since in theory, that would allow switch currents beyond the safe operating area of the device. I could use the LM2678, but I really want/need the current limit feature of the LM2679, so I'm hoping I can figure out what's happening.
Thanks for any help/guidance you can provide.
Regards,
Danilo