This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
For the SOT-223 package, the junction-to-case value appears not to be stated directly in the data sheet. Is there a specified value for this parameter, and can you indicate it?
Thanks in advance.
For LM340MP-5.0
θJC = 65.2°C/W
Where θJC refers to the thermal resistance between the junction and the top center of the package.
We caclulated junction temperature at 1 W power dissapation and case temperature 69.6 C and it is 134.8 C. I am a quality engineer and stated that it will reduce product reliability to operate near the maximum temperature limit. Our design engineers think that it is not a problem. Moreover, some devices are going to thermul shutdown, if power consumption increases for any reason. We would like to setup conference call with TI to discuss this device applicaiton.
I have sent a request to the Thermal lab for modeling of the Psi(jt) value for the LM340MP (SOT-223-4).
This would be proper benchmark to use to estimate the internal junction temperature (Tj) from the measured surface temperature (Tc).
Tj = Tc + ( Psi(jt) x Pdiss )
http://www.ti.com/lit/an/spra953b/spra953b.pdf
http://www.ti.com/general/docs/lit/getliterature.tsp?literatureNumber=sprabi3&fileType=pdf
The declared standard turn-time for a new request for thermal modeling is stated to be two (2) weeks, but typically it takes one week. Although, the up-coming US holiday (27-May) could add a day or two,
Results are back from the thermal modeling group for the LM340MP ...
Theta JA- (High K) = 60.2 °C/W
Theta JC, top = 42.1 °C/W
Theta JB = 8.9 °C/W
Psi JT = 2.7 °C/W
Psi JB = 8.8 °C/W