Hi, Chris
When I replied our conversation, It is disappeared. So. I made new conversation.
Anyway....
Question 1:
Finally I want to know that is it OK 1A continuously at 4.5V<Vin<5.5V without thermal fault
When I designed with recommended condition in the datasheet?
Question 2 :
And is it OK 1A continuously at 4.5V<Vin<5.5V without thermal fault in the Evaluation board?
In the datasheet, It seem to be OK. But it’s not plotted. <Refer to the below>