Hello,
I have to implement a DC/DC converter that inputs 8V-19V, and outputs 5V@10A. The LMZ13610 at first glance fits, but there are doc confusion : the data sheet gives an input range of 7..36V for 5V output, while the diagram on the web page gives 9..36V input range for 5V output, and webench claims the device is not applicable for the required input range ...
Could you please provide the min input voltage required for a 5V@10A output ?
Thanks !