This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Testing UCC25706 before implementing it into boost converter

Other Parts Discussed in Thread: UCC25706

Hi everybody

I have never used this kind of IC before and have never really fully designed a boost converter ethier. I thought this would be a great learning experience. With the power portion of the converter aside I had a few questions about the UCC25706 chip.

Here is a list of parameters for my circuit:

Vin(min): 36V

Vin(max): 49V

Vin(shutdown): 32V

Converter Frequency: roughly 300kHz

My circuit seems to work ok with the exception that when power is first applied to the circuit it takes almost five minutes for a PWM signal to appear on the OUT pin. There is also no output on the RC pin during this time. If I wait long enough the PWM signal, as well as the triangle wave on the RC pin, will appear. Not sure what is causing this. Any ideas? 

VDD on the 25706 is 11.7V. The start up voltage in the spec sheet states: 11.2 to 12.8. So my 11.7V on VDD should be ok.

I also want to know if I can use a 0 to 5V signal on the feedback pin, I have a pot connected to it now, to simulate what the chip will see when the power portion of the boost converter is connected to it?

Attached is the schematic of my current circuit. Please feel free to view and give feedback.

Thanks in advance,

Jesse

UCC25706.pdf