This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2 level dimming of LEDs using LM3463

Other Parts Discussed in Thread: LM3463

I am looking to drive 4 strings of LED at 100ma, ~21V.  I need to be able to provide 50% dimming when a room is sensed to be occupied via say an PIR.  Assume the input the circuit is a simple logic single and I want to be at either 100% or 50%.  I was looking at the LM3463 and using the analog dimming control, thinking that I could switch in a different resistor value to change the voltage at the Ioutadj pin.   Is this what you would recommend?