Hi all, I am planning a system of energy recovery. I use an electric motor in DC 24V - 250W, for supplying an electric bicycle. When the user operates the brakes, the engine shuts down and enters the circuit of energy recovery. I'm looking for a chip that will allow me to charge 8 cells LiFePO4 batteries, 3.2 V - 15Ah. The input voltage is between 9V and 30V DC. The coils are equipped with a control circuit and balancing (BMS).
Thanks to all those who want to help in the search of the chip.
best regards, Cesare Albanesi