Hi
I'm familiar with the old UC3879 but need some help wiht the UCC3895. I'm using peak-current control.
With 3879 you can't limit the maximum duty cycle. The linear part can be set but the circuit still jumps up to 100% duty cycle if for example the converter input voltage drops low. Can the 3895 be set to a maximum duty cycle by choosing the right oscillator C and R? I have timing problem above 97% duty cycle and want to avoid this operation point. Is the change from 3879 to 3895 a possible solution to my problem?