Hello. I'm fairly new to battery management, and 'd like to find the first thing to look at when the charger malfunctions.
Device: BQ24113A. Schematic: exaclty as is the datasheet's sample schematic. Charger: 9v 500mA walljack. Load: secondaty DCDC switcher, no load (~200mA startup current), no battery.
I have 2 boards, same schematic, ~same value (to my belief and to 5% tolerance) components, slightly different (to 2cm/1in trace lengths) layout.
The first board works OK (with the battery, or without). The BQ24113A on the second board stops running (no pulses @ the inductor) as soon as the secondary DCDC is switched on (output voltage drops to below 1v) and starts up again if that DCDC is switched back off. I have 2 copies of the "board 2" - same problem. If I connect the battery, the BQ24113A seems to run OK on the "board2" too.
So, where woold you look at at first? (at second ... :-) Please suggest.
Thank you.